Metal industry

Forging asset efficiency

Rizhao Steel
Due to the economic slowdown in China and the consequent fall in steel demand, the country’s steel industry is seeking new ways to reduce production costs. Evolution pays Rizhao Steel a visit. According to the World Steel Association, about 50 percent of global steel production is used in the housing and construction sector, making it the biggest consumer of steel today. China is the largest producer and consumer of steel in...
Continue Reading...
DryLube

Hot applications run longer with graphite

Many bearings operate in very high temperature environments – but few lubricants can withstand the heat. SKF has developed bearing...

On the plus side

The SKF BeyondZero portfolio is SKF’s answer to the challenges of the future. Today, global environmental concerns and constraints – not...

Typical application for self-aligning roller bearings: lignite open-pit mining in Germany.

Upgraded SKF Explorer self-aligning roller bearings extend service life

Driven by customer needs in ­challenging industrial applications, SKF developed an improved heat treatment  that is now used for the entire...

Rannveig Rist

Iceland's first lady of aluminiumEven though Rannveig Rist is the only woman to occupy the top post in a large...

China Celebrates The Lantern Festival

Strategic partnership agreement with CITIC Special Steel

News SKF has signed a strategic partnership agreement with CITIC Pacific Special Steel Co., Ltd (CITIC Special Steel) to further strengthen...

Steel going strong

Continuous casting company Sidmar N.V. of Belgium has eliminated unplanned downtime caused by bearing failures. This was accomplished by installing...

Skärmavbild 2011-11-08 kl. 21.44.23

Solutions for Severstal

A vast metallurgical corporation founded in the aftermath of World War II, Severstal shares a problem common to many industrial...

steel-green1

Fitting steel & green into the same sentence

The global steel industry faces a tough challenge: to meet higher demand by increased production, to reduce the negative environmental...

Heavy lifting1

Heavy lifting

At SSAB’s sheet steel mill in Luleå, Sweden, great care is given to the 15 overhead process cranes that transport and tip...