Engineering Competence

No wear anywhere

NoWearTM is a coated bearing type from SKF that lowers friction when sufficient lubrication cannot be guaranteed. Its coating is harder than standard steel and its friction coefficient can be compared to that of PTFE or molybdenum disulphide. As a result, smearing and boundary lubrication-induced wear are prevented.

Related Content

NoWearTM is a coated bearing type from SKF that lowers friction when sufficient lubrication cannot be guaranteed. Its coating is harder than standard steel and its friction coefficient can be compared to that of PTFE or molybdenum disulphide. As a result, smearing and boundary lubrication-induced wear are prevented.

In papermaking machines, for example, bearings in the calender rolls are prone to smearing because of zero-load situations. By using NoWear coated bearings, the smearing risk is eliminated. One paper mill that uses NoWear bearings has found bearing life has increased by a factor of at least 10. Other applications for the bearings include compressors and hydraulic machinery.

Keep me updated

Want to learn more about what is driving change in the engineering world? EVOLUTION helps you to stay up to date with emerging trends as well as the latest technology. Sign up for EVOLUTION updates to receive new content directly to your inbox.

Sign up