Engineering Competence

Swell solution

French technology firm Symétrie makes hexapods – parallel kinematic systems for testing products and simulating swell. The devices are in high demand for use in the space, naval and aeronautical industries, as well as for many other applications.

Related Content

Deep in the south of France lies the city of Nîmes, with its impressive ancient monuments. The city was founded by enterprising Romans, who showed great engineering skill in its construction, and today it is still home to stunning innovation. In the workshops of the high-tech company Symétrie, six-legged, articulated machines, known as hexapods, are being developed and built.

In 2001, Olivier Lapierre and partner Thierry Roux formed Symétrie after realizing the hexapods they had been working on at the French National Laboratory of Metrology and Tests could be adapted to other applications. “We took another direction – from high-measuring hexapods to high-precision positioning and dynamic-motion hexapods,” says Lapierre, who is now Symétrie’s CEO. “The flexibility in the parallel kinematics of a hexapod that could be infinitely scalable opened up new ways of using simulators in various fields.”

The pair was soon joined by a former colleague, Gilles Diolez, who came to the new company to fulfil his doctoral thesis centring on geometrical positioning in the construction of new robot tools. Today, Symétrie provides hexapod solutions for use in such industries as shipbuilding, aeronautics, automotive, optics, medical, nuclear and electronics, as well as in research centres. Hexapods incorporate six actuators and are capable of moving in any direction or orientation, generating strong and dynamic motions.

World’s largest hexapods

With extensive experience in factory automation, SKF Transrol specializes in ball and roller screws, and in electromechanical actuators. The company has long been at the forefront of developing electromechanical cylinders; today, its cylinders can match the power of hydraulics and the speed of pneumatics.

In 2003, Symétrie asked SKF for a quote on high-speed actuators with specifications well beyond the usual standards. Since then, further collaborations with Symétrie have taken SKF Transrol into new areas. The latest project involved construction of the two largest hexapods ever built. Running simultaneously, the hexapods simulate swell. They can reach five metres in height and operate within “six degrees of freedom” (movement and rotation on three perpendicular axes). Symétrie’s customer required that the hexapods be capable of powerful dynamic motion while carrying a weight of four tonnes. Designated EMC SLSA 50×50, the hexapod’s specially developed actuators can move at speeds of up to 1.5 metres per second, with a two-metre-long stroke and safety brake directly mounted onto the screw.

Customers often call on Symétrie to provide technical solutions that have never been produced before. To achieve this, the company works with parts suppliers that are both technically know­ledgeable and open to new ideas.

One such company is SKF Transrol, situated in Chambéry, France. SKF project manager Olivier­ Fernoux thoroughly embraced the challenge of integrating SKF actuators into a Symétrie hexapod. Lapierre recalls, “SKF showed us great interest and respect right from the beginning. It took a few volleys, and both sides progressed immensely.”

The result was the swell-simulating hexapod that was dubbed Sirocco after one of the many winds that blow through Nîmes. Symétrie’s customer, the French maritime engineering company GTT (Gaztransport & Technigaz), was impressed with Sirocco and in subsequent years acquired several other hexapods of various sizes to complete its test facilities. Symétrie’s swell-simulation hexapods enable GTT to study the impact of moving liquids onto the isolation membrane that GTT has designed for the maritime transport of liquid natural gas.

Today, Symétrie boasts a 20-strong team of engineers working on solutions involving mechanical, electronic and software engineering. Two-thirds of new recruits to the company come after completing their final exams at university.

The company’s workshops have recently been extended by 400 square metres to accommodate larger hexapods and test benches. Adjoining laboratories contain smaller hexapods, such as the Sures, a model used to position telescope mirrors with a precision of less than 0.1 micron in deviation.

Symétrie is expanding and looking for international development, but at the same time the company aims to retain the same corporate structure in order to stay flexible and inventive. Turnover grew by 50 percent between 2011 and 2012, increasing to 4.1 million euros.

Lapierre sees space applications as the next frontier for hexapods. “The next generation of space telescopes will have bigger mirrors that will need to be precisely positioned during operation,” he says.


Related Links

Keep me updated

Want to learn more about what is driving change in the engineering world? EVOLUTION helps you to stay up to date with emerging trends as well as the latest technology. Sign up for EVOLUTION updates to receive new content directly to your inbox.

Sign up