An ocean of power

An ocean of power

The MeyGen project in Pentland Firth, Scotland, is the world’s largest tidal-stream project to date. It will have a huge significance for the future of sustainable energy supply.

Text Sanja Bjelica
Photos Andritz Hydro

Electricity, gas and water supply Cylindrical roller bearings

Facts

Key Figures
Power generation capacity of 20 h/day
Rated power: 1.2–1.5 MW per turbine
Operating depth: 115 to 330 feet
Rotor nominal speed: 10–15 rpm
Generator nominal voltage: 6.6 kV

ANDRITZ HYDRO
ANDRITZ HYDRO Hammerfest (UK) and ANDRITZ HYDRO are part of the ANDRITZ GROUP.
ANDRITZ HYDRO is a global supplier of electro-mechanical systems and services for hydropower plants and a leader in the world market for hydraulic power generation.
Headquarters are in Vienna, Austria.
ANDRITZ HYDRO employs more than 7,500 people worldwide.
www.andritz.com/hydro

With climate change a pressing global threat to the world’s economy and environment, there is a strong need to deliver clean, renewable and sustainable energy. Tidal energy is one step toward a transition to a low-carbon economy and an increased renewable energy share for households and communities around the world.

Tidal energy is classified as an ocean technology that converts the energy caused by cyclical movements of the sea into electricity. There are three ways to generate electric energy from the tides; one of these is via underwater propellers (similar to windmills) powered by tidal streams.

Test-running of the turbine.

Test-running of the turbine.

The world’s largest planned tidal-stream project to date is the MeyGen project in Scotland’s inhospitable Pentland Firth. Here, ANDRITZ HYDRO Hammerfest, based in Glasgow (UK) and part of ANDRITZ HYDRO in Austria, is supplying three of the four turbines for the initial phase 1a. The project is considered to have the utmost significance for power generation and potentially for the future of sustainable energy supply. The turbines have a capacity of 1.5 megawatts each, and a rotational speed of 14 revolutions per minute. The plan is to have 270 turbines operating in 2020, at a full capacity of 398 MW.

This requires careful engineering, manufacturing and assembly, ensuring the reliable operation and high performance of the deployed technology.
Dr Carsten Hermann, of the Design and Development Department of Andritz Hydro in Ravensburg, Germany

The tidal turbines will be placed in the Inner Sound of the Pentland Firth, in the waters that separate the northern Scottish mainland from Stroma Island. It is home to whales and dolphins and other marine animals and is well known for its tidal streams, which are among the fastest in the world, with speeds of almost 11 miles per hour. With a suitable water depth of about 100 feet and very high flow velocity of about 15 feet per second, it is potentially one of the best spots worldwide for tidal power generation.

Assembly of two tidal turbine nacelles at the ANDRITZ HYDRO plant in Ravensburg, Germany.

Assembly of two tidal turbine nacelles at the ANDRITZ HYDRO plant in Ravensburg, Germany.

Nevertheless, the neighboring Atlantic Ocean with its rough conditions makes the Inner Sound of the Pentland Firth one of the most challenging maritime environments on earth. As such, it is a complex location for operation that requires state-of-the-art machinery. “This requires careful engineering, manufacturing and assembly, ensuring the reliable operation and high performance of the deployed technology,” says Dr. Carsten Hermann, of the Design and Development Department of ANDRITZ HYDRO in Ravensburg, Germany, where the turbines are manufactured. The components developed and delivered by ANDRITZ HYDRO have a predicted service life of about 25 years with a maintenance interval of five years.

Advances in tidal stream technology enable the production of a high degree of energy output. Few companies are developing expertise in this market, but ANDRITZ HYDRO has many years of experience in ocean technology. The company delivered and installed the entire electro-mechanical equipment for the world’s largest tidal power plant in Sihwa, South Korea. Most recently the company received an order for the rehabilitation of a tidal power plant in La Rance, France.

Assembling of the turbine main shaft. The front cover is being put into place. It incorporates a special seawater resistant seal, designed and supplied by SKF Marine.

Assembling of the turbine main shaft. The front cover is being put into place. It incorporates a special seawater resistant seal, designed and supplied by SKF Marine.

The design of the tidal turbines that are currently in production for the Penthland Firth is based upon the former prototypes that were tested in Kvalsund, Norway, installed in 2003 (300 kW) and at the European Marine Energy Centre, Orkney Islands, installed in 2011 (1,000 kW). In 2014 this development and know-how resulted in an order for the world’s first commercial tidal current power plant in Pentland Firth, Scotland.

A comprehensive offering

SKF has assisted ANDRITZ HYDRO with technical expertise, in particular in the design of the propeller shaft bearing arrangement, life calculations, both dynamic and static (safety) calculations, and the specific execution of the customized bearings. SKF also assisted with specific tools and specified mounting procedures for the propeller shaft bearings and a special front seal by SKF Marine.

Related content