Deep groove ball bearings

Upgraded SKF Explorer self-aligning roller bearings extend service life

Typical application for self-aligning roller bearings: lignite open-pit mining in Germany.
Driven by customer needs in challenging industrial applications, SKF developed an improved heat treatment  that is now used for the entire range of SKF self-aligning roller bearings (fig. 1). This  improved steel provides additional wear resist­ance while maintaining toughness, to potentially double bearing service life – particularly in applications where there are high levels of contamination or poor lubrication conditions. When SKF first launched the SKF Explorer performance class in 1999,...
Continue Reading...
SKF Drum Support Unit

How a new drum support unit saves energy

Saving energy and reducing ­manufacturing costs are the goals of the SKF Drum Support Unit for front loading washing machines. In...

SKF supplies bearings to Zytek’s hybrid-electric racing car

SKF supplies bearings to Zytek’s hybrid-electric racing car

  Zytek Engineering has chosen SKF to supply customized and standard deep groove ball bearings for the electric motor generator unit...

A hub of energy in Slovenia

A hub of energy in Slovenia

Two amateur Slovenian cyclists have become professional entrepreneurs, marketing a unique driving wheel hub to cycling enthusiasts around the world.     Everything...

Aiming high MISTRAL’S marvellous motor

Aiming high – MISTRAL’s marvellous motor

MISTRAL Engines has developed a new liquid-cooled, multi-fuel, electronically controlled rotary engine to meet the needs of 21st century general...

Installed confidence

Installed confidence

Agricultural machinery leads a hard life. Mud, water, dust and dirt make for rough working conditions, while inexpert users often...

Chopper challenge1

Chopper challenge

The dream of a helicopter of your own is coming closer to being realized, thanks to the self-build machines from...

Milking on demand1

Milking on demand

Milking machines from Swedish company DeLaval make it possible for cows to just about milk themselves. It is an ordinary Mondayat milk-machinery...

Riding the right wind 1

Riding the right wind

Bajaj Auto is confident that through an innovative R&D department and Japanese management methods it will regain its position as...

Monster warehouse trucks reach new levels6

Monster warehouse trucks reach new levels

Today’s warehouse trucks literally reach for the sky. Combining muscles with electronics, the new Vector C15 from BT Industries is...