Other (rolling bearings)
Rolling bearings TC 4 meets GPS TC 213
Small slewing bearings
In June 2001, SKF launched its new line of L-shape slewing bearings to cover small machinery applications ranging from aerial...
Wind power made easier
A new wind turbine simplifies the mechanics in machinery, bringing down maintenance costs considerably.If there is one aspect to modern,...
Maintenance-free universal joint bearings
SKF has developed universal joint bearings with a service life of 1 million kilometers (620,000 miles). The bearings eliminate the...
Fewer vibrations
Consumers are about to experience a revolution in their laundry rooms, thanks to the autobalancing technology from SKF Autobalance Systems....
The attraction of magnetic bearings
Active magnetic bearings mark a new era in combining electrical and mechanical systems. They offer considerable benefits in extreme high-speed...
Tilting toward the future
Part helicopter, part airplane, it will take off vertically yet be able to fly forward at high speed. The Bell...
SKF gets Ukraine bearing plant
SKF has acquired a majority holding in Lutsk Bearing Plant, one of the largest bearing manufacturing companies in Ukraine. ...
Magnetic partners
SKF and Calgary-based Revolve Technologies Inc. in Canada have established a new company, Revolve Magnetic Bearings Inc. "With this alliance,...
The maintenance-free universal joint
The universal joint for commercial vehicle propeller shafts is essentially a specially-designed grease-lubricated needle roller bearing. This new maintenance-free universal...