Spherical roller bearings
Premature bearing failures in wind gearboxes and white etching cracks (WEC)
Upgraded SKF Explorer self-aligning roller bearings extend service life
Driven by customer needs in challenging industrial applications, SKF developed an improved heat treatment that is now used for the...
In the kiln zone
When Belgian mining company Argex wanted to replace the support roller units on its rotary kiln, it looked to long-time...
Boldrini likes it hot … and cold
Some like it hot, as in the classic Marilyn Monroe movie of that name. And some like it cold. Italian...
The big bend
Swiss company Haeusler AG sets the global standard for metal-bending machinery. The forces in these huge machines require bearings that...
Eager to learn
Colombia-based Drypers Andina is a young company that’s eager to learn, and working with SKF helps it to do just...
Installed confidence
Agricultural machinery leads a hard life. Mud, water, dust and dirt make for rough working conditions, while inexpert users often...
Chopper challenge
The dream of a helicopter of your own is coming closer to being realized, thanks to the self-build machines from...
Design away lubrication
SKF lubrication-free components offer advantages for Off-Highway vehicles. Off-Highway vehiclesused in the construction, agricultural, and forestry industries face harsh conditions that...
Power to spare
In ports up and down the East Coast and the Gulf of Mexico, Moran Towing guides ships safely to their...