Cool running

Cool running

Transporting iron ore by rail is a critical aspect of mining in the Arctic Circle. And predictive maintenance is a critical aspect of keeping the Iron Ore Line running smoothly and reliably in the region’s extreme climatic conditions.

Summary

LKAB

– LKAB (Luossavaara-Kiirunavaara AB)

– Business: The company is a high-tech international minerals group, world-leading producer of processed iron ore products for steelmaking and a growing supplier of mineral products for other industrial sectors.

– Markets: The majority of the iron ore products are sold to European steelworks, with other important markets including North Africa, the Middle East and Southeast Asia. Sales of industrial minerals take place chiefly in Europe and to growing markets in Asia and the USA.

– Sales: 27 billion Swedish kronor in 2012 ($4.1 billion)

– Employees: 4,200 people in 2012

www.lkab.com

Related Links

SKF Insight

LKAB

Self-aligning ball bearings

Cylindrical roller bearings

Tapered roller bearings

Sales Contact

Camilla Svensson, Camilla.Svensson@skf.com

During the winter months, temperatures can drop as low as –40 degrees Fahrenheit in Kiruna, situated north of the Arctic Circle in Swedish Lapland. The town is home to the world’s largest underground iron ore mine, operated by LKAB, a world-leading producer of processed iron ore products.

Despite these extreme weather conditions, millions of tons of iron ore are transported every year along the 300-mile-long Iron Ore Line. The world’s strongest locomotives haul ore from Kiruna to harbor storage depots in Luleå to the south and to Narvik, Norway, in the northwest. This railroad is the backbone of the northern mining industry and has been since its beginning more than a century ago.

Iron ore was discovered in the region in the 1600s, but because of the remote location and harsh climate, no mining was initiated until the 1800s. At that time, small amounts of ore were extracted during the summer months and then transported in the winter using horse- and reindeer-drawn sleds.

“The idea at first was to use balloons to transport the iron ore, but that didn’t work,” says Thomas Nordmark, manager R&D Railroad, LKAB. “Later, the Sami people got involved with their reindeers and the sleds, but it wasn’t until the railway came along that the iron ore operation really took off here.”

That was in 1888, a decade after a process was developed to separate phosphorus from the ore. An English company built the first section of the ore railway between Malmberget in Gällivare municipality and the newly built ore harbor in Luleå. The railway was eventually sold to the Swedish state. In 1890 the government founded LKAB (Luossavaara-Kiirunavaara Aktiebolag), and plans to expand the railway were set in motion.

At the turn of the century the Iron Ore Line was linked to Narvik, making it the world’s northernmost railroad. LKAB’s entire mining operation was linked via railways to its global markets. Efficient transportation from the mines to its steel industry customers across Europe was, and still is, crucial to LKAB’s success. The mining company is responsible for 90 percent of the iron ore production within the European Union.

Today IORE locomotives builT by Bombardier Transportation and hauling 68 ore cars, each with a load capacity of 110 tons, leave the Kiruna mine every other hour headed for the storage depots at Narvik or Luleå.

“Without the railway logistics system we could never deliver the volumes of iron ore that we produce at LKAB,” says David Lövgren, senior manager Maintenance Technology, LKAB. “Annually, we produce and transport 30 million tons of iron ore at LKAB.”

LKAB has a target to increase that annual figure to 41 million tons by 2015, a target that puts big demands on suppliers’ products and solutions to withstand the extra loads and the wear and tear.

Two main issues for the railway are the wheelset bearings, which must handle very heavy axle loads, and the lubricant and sealing that must stand up to the cold temperatures. SKF worked with LKAB to develop a new type of sealing solution specially designed to withstand the harsh climate.

As for wheelset bearings, SKF bearings have been helping LKAB’s wagons roll since 1913.

The first trials with SKF self-aligning ball bearings were made at the Malmberget mine. Today’s freight wagon wheelsets feature compact tapered roller bearing units. After about 500,000 miles of use, the bearing units are removed and sent to the SKF refurbishment center in Gothenburg. The bearing units are dismantled, cleaned, analyzed, filled with new grease and fitted with a new sealing solution before being put back to service.

The new seal, used in the tapered roller bearing units, operates with lower friction than previous designs and contributes to LKAB’s full train energy reduction target. LKAB aims to reduce its overall energy consumption in its operations by 2 percent.

“We consider ourselves very energy efficient,” Nordmark says. “We have quite new locomotives that are regenerating energy back to the network when the brakes are applied to the train. With an 9,400-ton train, you’re feeding a lot of power back into the engine, so in total we save about 25 percent of the energy used for one trip between Kiruna and Narvik.”
On a single track, the trains must run reliably and without any breakdown. In addition to having equipment  that is efficient and durable, it is essential to be one step ahead – to locate problems and stop the train before failure occurs. LKAB uses a predictive maintenance plan to do just that.

“Within LKAB Malmtrafik, we use a predictive maintenance program that helps plan the appropriate maintenance for our locomotives and railcars, depending on how long they’ve traveled,” Lövgren explains. “Condition monitoring with tools such as vibration analysis is used to ensure that our equipment has a high level of availability and reliability.”

The remote condition monitoring of locomotives is still in the early stages, but it is on track to becoming the future of train maintenance. SKF works closely with LKAB on condition monitoring of assets, using a variety of technologies including SKF Insight, an innovation in intelligent wireless technologies that is integrated into SKF bearings (see image on page 2).

LKAB has invested more than 5 billion Swedish kronor ($770 million) over the past decade in new locomotives, railcars and expansion of rail terminals. Today the priority is to use new technology and solutions to keep the Iron Ore Line operating reliably into the future.

SKF Insight is a trademark of the SKF Group

SKF’s contribution to the Iron Ore Line

Locomotives:

  • Wheelset bearings
  • Traction motor bearings
  • Gearbox (transmission) bearings

Freight wagons:

  • Wheelset bearings
  • Wheelset bearings with new low friction seal

Services:

  • Refurbishment of wheelset bearings for the freight cars
  • Condition monitoring: IMx + analysis
  • Bearing investigation.

Related content