Zellstoff Celgar

No time to waste

The pulp and paper industry can conjure up images of black smoke, dirty rivers and forest clear-cutting. But one Canadian company is working hard to change those industry stereotypes. Mercer International runs three of the greenest northern bleached softwood kraft pulp mills in the world, including Zellstoff Celgar, just outside the town of Castlegar in British Columbia.

Text Stephanie Johansson Photo Peter Moynes

Condition monitoring Pulp and paper Reliability

Facts

SKF’s custom-made predictive maintenance

Since 2006, SKF’s asset management services have been at work inside the Zellstoff Celgar mill, helping to increase reliability and availability of critical machines.

“Before, preventive maintenance was used,” says Jose Rabell, project manager PdM Services. “This, in fact, is more expensive than predictive maintenance. They used to lubricate based on time, according to a schedule. They couldn’t predict what was happening. Today they take a vibration reading and lubricate only when needed.”

More than 70 pieces of SKF hardware are at work inside the Celgar mill: online systems with wireless units, wired units, handhelds and protection systems on the turbines. Some 250,000 readings are processed and analyzed daily with the SKF @ptitude decision support software.

SKF’s service and support helped Celgar reach an unheard-of achievement in the industry – zero unpredicted maintenance failures in 2012.

@ptitude is a registered trademark of the SKF Group 

 

Related Links

Zellstoff Celgar

Sales Contact

Walter Del Degan, Walter.Del.Degan@skf.com

In western Canada, Zellstoff Celgar’s name is synonymous not only with premium-grade kraft pulp used in a range of products such as tissue and writing paper, but also with bioenergy.

Zellstoff Celgar uses residual fiber – what is known as waste wood – in the pulp-making process. It is cooked in a digester to break down the lignin that holds the wood together. Half of what is left becomes cellulose pulp, which is used to make paper. The other half is black liquor, essentially a biofuel. This black liquor is burned in the mill’s modern recovery boiler to generate power – renewable bioenergy.

Wood is considered carbon-neutral, and energy produced from wood is therefore labeled “green,” as opposed to the “brown” energy produced from nonrenewable coal.

“We really started producing bioenergy on the day the mill started in 1961,” explains Ralph Lunn, process engineering manager at Zellstoff Celgar. “When pulp is made, lignin is released, recovered and burned in a boiler. The steam produced by the boiler is sent to a turbine to generate electricity or produce bioenergy. In 1993 the mill underwent a significant capacity expansion from about 600 tons per day to 1,200 tons per day, which increased the amount of lignin recovered and burned by a similar ratio.”

Lunn, who has been with the mill since 1992, is responsible for bio products, R&D and energy. He has seen firsthand the investments through the years that have increased mill production and thereby the amount of bioenergy produced.

For several years the mill did not have the turbine capacity to utilize the additional steam produced, so it was simply vented into the atmosphere. To change this and to produce more bioenergy, a new turbine was installed in 2010. This became the Green Energy Project.

“This was a $61 million project, which included the installation of a second turbine-generator set with a design capacity of 48 megawatts,” Lunn says. “This increased the mill’s installed generating capacity to 100 megawatts and upgrade the mill’s bark boiler and steam facilities.”
The investment made Celgar the largest single-line mill in Canada.

Financing for the project came from Celgar’s parent company, Mercer International, and from the Canadian government through its Pulp and Paper Green Transformation Program. The program supports capital projects that conserve or produce energy or reduce environmental impact. It was created in response to the black-liquor tax credit that the United States had offered U.S. companies.

At this time, Celgar also finalized a 10-year electricity purchase agreement with BC Hydro, a local utility company, to sell its excess energy at favorable green-energy rates. The mill produces approximately 520,000 megawatt-hours annually, but only about 340,000 megawatt-hours of that electricity is used internally; the remainder is fed into BC Hydro’s grid, powering more than 16,000 local homes.

Lunn says the mill currently utilizes about 65 megawatts of its 100 megawatts total turbine capacity, so there is room for additional power generation.

“This will require more steam production, less steam usage in the mill, or both,” he continues. “We are constantly on the lookout for ways to save steam in the mill, but increased steam production is likely a more capital-intensive proposition.”

Celgar has several by-products in the mill that are part of the existing process, so Lunn and his colleagues are investigating ways to recover value from those products. Examples include fly ash from the hog fuel boiler, methanol from condensates and turpentine from the black liquor.

For Celgar, being a truly green company means thinking sustainably through the entire value chain. The mill is very strict with its suppliers, accepting only sustainably harvested, certified wood. When it comes to production, Celgar’s efficiency and operational excellence are recognized through its ISO 9001 and ISO 14001 certifications for quality and environment. The company is also actively working with the transportation industry to lower its carbon footprint. One step in the right direction is the recent 15 percent increase in the size of chip trucks, which means 15 percent fewer trucks on the road.

With the stereotype of pulp mills as a dirty business still hanging overhead, the Celgar team hopes its work to educate the community and raise awareness is changing minds.

“It is important to know that most of the white ‘smoke’ coming out of the stacks is actually water vapor,” says Lunn. “Anything else is treated with various scrubbing technologies to minimize what goes to the air, which is necessary to meet the mill’s stringent environmental permit requirements.”

Download the Evolution iPad app to watch a video about SKF’s contribution to Zellstoff Celgar.

Related content