Wheels set to last

Wheels set to last

A new revolutionary material developed by GHH-BONATRANS will boost reliability and reduce life-cycle costs of railway wheelsets.

Text James Drake
Photos Stadler, Vladimir Weiss

Bearing units Industry Railways

The next time you find yourself traveling by train and listening to the clatter of the wheels, take a moment to think about the skill and expertise of the people who made them.
        

Sales contact

evolution@skf.com

“Locomotive wheels are exposed to huge loads,” says Marcel Ujfaluši, head of business development and marketing for GHH-BONATRANS, one of the world’s leading manufacturers of railway wheelsets.

The contact zone between wheel and rail is no bigger than the surface area of a one-euro coin, he explains, and that area has to support both the weight and guiding forces of the train, as well as transfer the traction power. “If those wheels are going to be able to take the strains, we have to use first-class materials,” he says.

The benefits don’t stop at harder wheels.
Peter JanoŠ, GHH-BONATRANS LCC manager

Ujfaluši knows what he’s talking about. From its base in the town of Bohumín, tucked away in the northeast corner of the Czech Republic, GHH-BONATRANS’ delivers wheelsets to major railway companies and rolling stock producers all over the world.

Leading wheelset designer

BONASTAR®4BD is dedicated primarily to locomotive wheels and axle sets, but GHH-BONATRANS has developed the material to suit all types of passenger and freight wheelsets – high-speed intercity and regional trains, suburban and light rail vehicles, underground trains and freight wagons.

As a leading European wheelset designer and manufacturer, GHH-BONATRANS supplies a full range of products and solutions, such as heavy rail wheelsets for high-speed trains and locomotives and low-floor solutions for light rail, including resilient wheels and noise-absorbing solutions.

Wheelsets for passenger trains

Wheelsets for passenger trains at the Bonatrans production plant.

Meeting the challenge

With SKF’s TBUs, grease life is a crucial part of extending the interval between overhauls to 1 million miles. Bearing grease life depends on various factors, such as operating temperature, rotational speed, bearing size and cleanliness. “The challenge was to find a way of reducing friction to obtain cooler running and at the same time avoiding wear and tear, without negatively affecting the strength of the material or bearing service life,” says Jan Babka, senior SKF railway industry business engineer.

Continuous design and manufacturing improvements have resulted in substantial reduction of the frictional moment in the bearing unit, and an optimized sealing arrangement keeps contaminants out of the bearing.

To minimize wear, SKF applies its patented Xbite heat treatment technology to the bearing rings. With Xbite, the same hardness as conventional martensite hardening is obtained, but important additional benefits are higher toughness levels and extended fatigue life.

From the beginning of its 200-year history, GHH-BONATRANS’ reputation for excellence has gone hand in hand with the attention it pays to safety and dependability. But preserving that reputation has never come easily. Successive generations of engineers from GHH-BONATRANS have struggled to reduce the life-cycle cost (LCC) of their wheelsets without compromising on performance.

Now GHH-BONATRANS’ research engineers are convinced that their latest development marks a quantum leap for the industry. The specially developed material is BONASTAR®4BD – a revolutionary wheel material that delivers 30 percent longer life in mileage terms, compared with wheels made of standard steel grades.

BONASTAR®4BD enables greater resistance against rolling contact fatigue (the process of fatigue caused by rolling/sliding contact) and hence against the development of deformations on the wheel tread. Ultimately that both boosts reliability and reduces wheelset LCC.

Mounting a TBU on a wheelset.

Mounting a TBU on a wheelset.

GHH-BONATRANS LCC Manager Petr Janoš does not reveal the details of the newly patented technology, but he is happy to describe its benefits. “We looked at different chemical compositions, and we tested different varieties of heat treatment – the use of heating or chilling to extreme temperatures – to achieve added hardening,” he says. “But the benefits don’t stop at harder wheels.”

Indeed they don’t. The longstanding relationship between GHH-BONATRANS and SKF, which supplies tapered rolling bearing units (TBUs), has led to a technological marriage of minds that promises to lower LCC still further by minimizing the frequency of maintenance.

“Cutting the number of overhauls for a bogie during the life of a train is key to reducing LCC,” says Jan Babka, senior SKF railway industry business engineer.

Mounting a TBU on a wheelset.

Mounting a TBU on a wheelset.

SKF’s TBUs operate for as much as 1 million miles between overhauls. This allows for bearing overhaul intervals that coincide with those of wheels made from BONASTAR®4BD.

Continuous improvements to SKF TBUs have enabled SKF to reduce the frictional moment in the bearing by 30 percent. Lower operating temperatures lead to longer service life of the grease and hence extend maintenance intervals considerably in order to meet the wheelset maintenance intervals.

That will deliver considerable savings to the end user, says Babka. The combination of BONASTAR®4BD and SKF’s TBUs enables railway operators to extend the service interval and bring savings of as much as $3,500 per bogie per year, he says.

Related content