SKF stroboscopes
News
News
The new TKRS 10 and TKRS 20 SKF stroboscope range enables both maintenance technicians and machine operators to have a portable handheld stroboscope that meets their needs.
The stroboscopes use LED technology to enable a high flash rate with a very low power consumption. They also have a number of features that will be appreciated by many users, such as flash rate memories and connectivity to SKF Microlog. Unlike other handheld portable stroboscopes, the TKRS 10 and TKRS 20 are supplied with a remote laser sensor. This enables the flash rate to be easily triggered and also allows the stroboscope to be used as a tachometer.