Engineering Competence
Record-setting sealed bearing

Record-setting sealed bearing

Related Content

SKF’s bearing factory in Gothenburg, Sweden, has produced the company’s largest sealed spherical roller bearing to date. The 241/900 spherical roller bearing is 50 percent larger and three times heavier than the previous largest SKF sealed spherical roller bearing.

Destined for a Polysius Polycom 8 roller press at a large copper mine in Peru, the three-tonne heavy spherical roller bearing is dimensionally equivalent to the standard SKF non-sealed version, with a bore diameter of 900 millimetres, an outside diameter of 1,420 millimetres and a width of 515 millimetres. The bearing seal consists of a rubber over-moulded steel plate with the same profile and offering the same characteristics as those currently used with existing SKF sealed spherical roller bearings.

The bearings will be fitted to a horizontal shaft and will operate in extremely dusty conditions. The roller press is a heavy-load application subject to frequent shock loading; the predominantly radial loads, when coupled with the high level of contamination at the site, pose a significant risk of early bearing damage and failure. SKF’s custom-made seal aims to at least double the bearing service life by significantly reduc­ing the risk of contamination in this application.

Keep me updated

Want to learn more about what is driving change in the engineering world? EVOLUTION helps you to stay up to date with emerging trends as well as the latest technology. Sign up for EVOLUTION updates to receive new content directly to your inbox.

Sign up