Industry
Orbital Marine’s SR2000 tidal turbine on site at the European Marine Energy Centre, Orkney.

Turning the tide

Tidal energy has been identified as a potentially important global source of sustainable renewable energy. A Scottish company and SKF are collaborating on a joint project to use floating tidal turbine technology to reduce the costs of generating electricity.

Related Content

Orbital Marine Power Ltd., a leading Scottish tidal turbine device developer, has commercial applications of tidal energy squarely in its sights. Orbital Marine’s goal, says company CEO Andrew Scott, is to “see tidal energy grow into a commercial industry and provide a new source of renewable energy to the global market”. The market potential for tidal energy exceeds 100 gigawatts, he says, explaining that the constraints on harnessing tidal energy have really revolved around the cost of technologies to capture it. “This is something we are setting out to change,” Scott says.

Orbital

Orbital Marine Power Ltd. was founded in 2002.

The company has 26 employees at offices in Orkney and Edinburgh.

In 2016 its first milestone was the SR2000 – the world’s most powerful tidal stream turbine at the time, which generated more than three gigawatt-hours of electricity over its initial 12 months of testing.

www.orbitalmarine.com

Essentially, the basic drivetrain components and system configuration are similar to those of a wind turbine, although the technology must withstand a dense and wet environment. “The real difference is around what you mount your nacelle to, and in that context our floating platform serves the same function as a wind turbine tower,” says Scott. “It’s more sophisticated because it has to deal with the challenges of the harsh marine environment in a tidal stream.”
The twin turbines are mounted onto retractable legs that are fixed to a floating platform, enabling the turbines to be positioned in the most energetic parts of the tidal stream.
A simplified structure helps to limit manufacturing expenditure.
The platform and blade configuration cater to sites and projects of differing characteristics and scale.

European Ocean Energy ERA-NET

Ocean Energy ERA-NET coordinates funding programmes between European countries and regions related to ocean energy research and innovation. The aim is to help maintain and grow Europe’s world-leading position in ocean energy, bring innovative, low-carbon energy solutions closer to commercial deployment, reduce energy costs and create growth and jobs. Eight national and regional government agencies have received funding from the European Union under the Horizon 2020 Programme for Research and Innovation. They are the Basque Country in Spain, Brittany and Pays de la Loire in France, as well as Ireland, Portugal, Scotland, Spain and Sweden. The project brings together Orbital’s core supply chain and strategic partners to deliver a future-proofed product solution with a much-reduced risk profile that is easier to finance.

One key to the commercialization of tidal turbines is the development of a pitch controller for the tidal turbine blades. “We are targeting up to a 50 percent increase in yield from our machines, bringing our performance firmly in line with more established technologies,” says Scott. The European Ocean Energy ERA-NET Cofund (see fact box) has given a 1.2 million euro research grant towards the development and delivery of the pitch controller, which is being integrated into Orbital’s new floating tidal turbine, the Orbital O2 2MW.

One key to the commercialization of tidal turbines is the development of a pitch controller for the tidal turbine blades. “We are targeting up to a 50 percent increase in yield from our machines, bringing our performance firmly in line with more established technologies,” says Scott. The European Ocean Energy ERA-NET Cofund (see fact box) has given a 1.2 million euro research grant towards the development and delivery of the pitch controller, which is being integrated into Orbital’s new floating tidal turbine, the Orbital O2 2MW.

We are targeting up to a 50 percent increase in yield from our machines.

Andrew Scott
CEO

“The easiest way for us to reduce the overall cost of energy is by being able to use longer rotor blades so they capture more energy from the tidal current,” Scott explains. “However, as the blades get longer the resulting loads become heavier and more challenging. A pitch controller system enables us to feather the blades such that we can control those loads far more accurately – an important solution to improve the economics of tidal energy.”

Because the technology is floating, all components and systems are readily accessible for maintenance, inspection and repair with minimal downtime, using only standard vessels. The technology is installed similarly to mooring a ship on a simple anchor arrangement, Scott says. “Alternative technologies with similar installed capacity fixed to the seabed are locked into using expensive vessels and equipment to recover them as they can’t be accessed while they’re fixed to the seabed,” he says. “This leads to a secondary problem of long periods of outages to access, recover and then repair turbines. Our costs are a fraction of our competitors’, and ultimately a totally different risk profile for investors and the supply chain.”

We will see markets grow as investors and governments increase their confidence and awareness of the solution that tidal energy can offer.

Andrew Scott
CEO

The turbine has been tested at the European Marine Energy Centre on the Orkney Islands, north of the Scottish mainland. “The Orkney Islands have a massive tidal stream resource, also known as the ‘Saudi Arabia of Tidal Power’,” says Scott. “The turbine was installed onto an existing subsea cable in one of the main tidal stream locations in Orkney, which let us export power to the local grid. This has been the test ground for the technology to operate in and provide all the valuable data required to validate performance, with the plan being to operate it for up to 15 years so we get good data sets for longer-term reliability and performance.”

Scott explains that the project will help Orbital Marine build experience and apply that to the engineering process to reduce costs. “In parallel,” he says, “we will see markets grow as investors and governments increase their confidence and awareness of the solution tidal energy can offer.”

Orbital Marine’s SR2000 tidal turbine

SKF pitch-control modules

The pitch-control modules for the Orbital Marine technology will be delivered by SKF’s advanced solutions factory in Gothenburg, Sweden. The controller rotates two sets of blades with 20-metre rotor diameters about their longitudinal axis. The flow profile can adapt to the ­existing tidal stream speeds. By regulating the angle of attack, a constant power input above the rated tidal stream speed can be realized.

Michael Baumann, Business Develop-ment Manager for Marine and Ocean Energy at SKF, says, “Our dedicated Ocean Energy team works collaboratively with the most advanced tidal turbine prototype device developers and sub-component suppliers to help them design in reliability at an early stage.” Because wind turbines and ship propulsion systems such as electrical pods have similar challenges to overcome, SKF can bring this technical knowledge to tidal stream turbine applications.

Direct benefits include improved control of drivetrain torque forces, facilitating a 50 percent increase in the swept area of the device (16- to 20-metre rotor diameter) and resulting in a similar level of yield increase to Orbital’s current turbine configuration. It offers enhanced blade control around the rated speed to reduce power shedding and smooth power fluctuations, lowering extreme loading and fatigue on the drivetrain and structure, with increased environmental shutdown limits and the ability to continue generation in the event of a minor malfunction.

SKF has worked with Orbital Marine on a range of small- and large-scale demonstrator turbines, including the record-breaking SR2000. “SKF sees tremendous potential in floating tidal technology, due to its low installation and operating costs,” says Baumann. “We’re delighted to be bringing our experience to bear in delivering a key enabling solution to drive cost reductions and accelerate the rollout of Orbital Marine’s floating tidal technology.”

Keep me updated

Want to learn more about what is driving change in the engineering world? EVOLUTION helps you to stay up to date with emerging trends as well as the latest technology. Sign up for EVOLUTION updates to receive new content directly to your inbox.

Sign up