SKF Explorer spherical roller thrust bearings boost ….

Another  bearing type has been added to the SKF Explorer class of high-performance products.

Related Content

The addition of spherical roller thrust bearings to the SKF Explorer class enables design and maintenance engineers to create SKF Explorer-quality bearing arrangements that will increase service life and reduce maintenance.

By design, a spherical roller thrust bearing is the only roller thrust bearing that can accommodate substantial radial loads in addition to thrust loads. This makes spherical roller thrust bearings an outstanding solution in applications where there are combined loads. This ability to accommodate combined loads enables economical, space-saving designs that can also provide a high degree of stiffness under heavy load conditions. Spherical roller thrust bearings are also the only thrust bearings that can accommodate shaft deflections and up to two or three degrees of misalignment between shaft and housing, depending on the bearing series.

SKF Explorer class bearings
SKF Explorer is a new performance class of rolling element bearings that provides a substantial improvement in key operational parameters relevant to the bearing type and its typical applications. This new level of performance represents the blending of SKF’s application knowledge with its expertise in tribology, materials development, design optimization,
manufacturing and not least a basically sound bearing design.

By studying the interrelationship between each bearing component, SKF engineers were able to maximize the effects of lubrication and minimize the effects of friction, wear and contamination. The research team looked at each component at the micro level and then developed new procedures to consistently manufacture to this new standard of excellence.

SKF Explorer spherical roller thrust bearings are characterized by a number of technical improvements, some of which are listed below.

  • Improved bearing steel – SKF Explorer spherical roller thrust bearings feature an ultra-clean, homogenous steel with an extremely low oxygen content, which increases bearing service life.
  • The unique SKF heat-treatment process– To maximize the benefits of SKF’s
  • ultra-clean steel, engineers incorporated unique heat-treatment procedures. These new procedures increase the bearing’s wear resistance while maintaining toughness and heat stabilization.
  • Improved surface finish – The surface finish on all contact surfaces has been improved to maximize the effects of the lubricant. This has led to a smoother, cooler-running bearing that lasts longer.

All in all, the performance for spherical roller thrust bearings were improved dramatically, and service life was far beyond ISO standard life predictions. SKF engineers therefore adjusted calculation parameters.

Increased design effectiveness
Spherical roller thrust bearings were developed by SKF in the 1930s for use in the oil industry, and by the 1940s they were incorporated in heavy applications such as railway turntables and pivot systems for bridges and cranes. They were particularly popular in those applications because of their high load-carrying capability over such a relatively small bearing volume.

Today, spherical roller thrust bearings are used in many different applications such as extruders, injection molding machinery, industrial gearboxes, water jets, thrusters, refiners, pumps, pivot bridges and cranes. One of the most illustrative examples of an SKF Explorer spherical roller thrust bearings is the azimuthing thruster, found in heavy-duty marine applications such as tug or harbor boats. They can also be found in the new pods – the revolutionary new propulsion system that combines an electric motor, shaft and propeller to propel and steer a ship. These are in service in cruise ships and even in large icebreakers (For more information, see Evolution issue 1/02 or visit evolution.skf.com).

In the ferry boat thruster application shown in this article, a constant 85 kN radial load is applied to the bearing arrangement. At full forward, a 170 kN thrust load is applied for 75% of the time and a 127 kN thrust load is applied in reverse for 25% of the time.

To accommodate these loads, design engineers have a choice with SKF Explorer spherical roller thrust bearings that they did not have in the past: They can either “power up” or “size down” the application.

Marine thruster arrangement
A common bearing arrangement for this type of thruster uses three bearings: two thrust bearings and one radial bearing. The two thrust bearings are “directional” – one is for forward, the other is for reverse. The radial bearing, as its name implies, is in the arrangement to accommodate the radial load.

For example, a common three-bearing arrangement incorporated a standard 23038 CC/W33 spherical roller bearing and two standard 29338 E spherical roller thrust bearings. Based on normal operating conditions, this arrangement should provide approximately 80,000 hours of reliable service.

Now, compare the calculated life of that same application using the same size SKF Explorer bearings in all three positions; the life of bearings will reach almost 200,000 hours.

As demonstrated, there is a dramatic improvement in the capability of the bearing arrangement, which opens up new possibilities to the design engineer. The options are either to increase the service life of the bearing arrangement, as was demonstrated above, increase power output or downsize the application for a more compact, more cost-effective solution. Let’s see how SKF application engineers were able to “size down” the application.

New design option
Look at the following example. The thrusters have been redesigned with just two SKF Explorer spherical roller thrust bearings having the same size as in the previous example. The 23038 CC/W33 spherical roller bearing was eliminated because spherical roller thrust bearings can accommodate radial loads in addition to thrust loads. The new two-bearing arrangement will provide more than 45,000 hours of reliable service. That’s almost five years of continuous operation under normal operating conditions. This exceeds the 40,000 hours required by the classification societies.

In oil-bath applications such as the one described above, the rollers in a spherical roller thrust bearing create a pumping action to provide the rollers with a continuous supply of lubricant. In addition to lubricating the contact surfaces of the bearing, this pumping action is an effective way to introduce a constant supply of oil to dissipate heat. Both of these characteristics can have a substantial impact on the service life of the bearing.

System lives were calculated using proprietary SKF software using advanced life-calculation methods.

SKF Explorer spherical roller thrust bearings provide advantages other than the most obvious ones in this example, e.g., downsizing and possibly eliminating another bearing. With SKF Explorer spherical roller thrust bearings and other bearings from the SKF Explorer class, it will be possible to realize new performance limits for all types of applications.

 

 

 

 

Keep me updated

Want to learn more about what is driving change in the engineering world? EVOLUTION helps you to stay up to date with emerging trends as well as the latest technology. Sign up for EVOLUTION updates to receive new content directly to your inbox.

Sign up