SKF Rolling Knowledge webinars

SKF GBLM – A new rating life model applied to hybrid bearings

Hybrid bearings are the preferred choice for high-speed, high-precision equipment such as machine tool spindles. By combining low weight, good electrical resistance and good performance under demanding lubrication and contamination conditions they are a perfect fit for many new applications, from electric vehicle powertrains to industrial pumps and compressors. Engineers know from experience that hybrid bearings can perform extremely well in these applications, lasting many times longer than their conventional all-steel counterparts.

Related Content

Until now, it has been difficult for engineers to predict whether a hybrid bearing will outperform a steel one in a given application, or whether the possible performance benefits that hybrid bearings enable are worth the extra investment they require. The conventional equations engineers use to calculate the rating life of a bearing do not reflect the real-world performance of hybrid designs. To rectify this issue, SKF developed what would become the Generalized Bearing Life Model, or GBLM.

Using GBLM, SKF engineers have been able to determine the real-world benefits hybrid bearings can have. In the case of a poorly lubricated pump bearing, for instance, the rating life of a hybrid bearing can be up to eight times that of a steel equivalent. In an electric motor, the Hybrid variant lasted 28% longer than the all-steel DGBB.

Listen to the GBLM Webinar
Listen to SKF expert Albrecht Nestle talking about the limitations of existing bearing rating life models for hybrid bearings and how and how the new Generalized Bearing Life Model solves this issue.

Keep me updated

Want to learn more about what is driving change in the engineering world? EVOLUTION helps you to stay up to date with emerging trends as well as the latest technology. Sign up for EVOLUTION updates to receive new content directly to your inbox.

Sign up