The future of bearing mounting
Bearing mounting is one of the most important aspects of bearing performance and service life. Estimates are that as many as 1 out of 6 premature bearing failures in industrial applications are related to mounting and handling errors. Now, thanks to a new digital tool, many of these can be avoided.
First of all, a correctly mounted bearing requires a certain amount of preparation. For one, you have to identify the correct bearing type, size and variant. It’s also important to know how the bearing was stored – hopefully on shelves not subjected to vibration, in a dry area, in its original and unopened package safe from contamination and corrosion. Further, you need a mounting environment where the bearing is adequately protected from humidity, dust, swarf and other debris resulting from machining processes.
Another crucial step is figuring out the correct order of assembly of the various components. In addition, there might be particular lubrication requirements involved, detailing what kind of lubricant you need, and the exact quantity. When you’re finally ready to mount – when you have all the necessary parts, tools, equipment and data at hand – you have to be confident that you have selected the appropriate mounting method. Are you using the basic mechanical methods of cold mounting, or the more refined oil injection method? Or is hot mounting required for your particular asset? Considering the intricacies involved in bearing mounting, it’s clear that quick access to proper information is crucial.
Being recognized as a leader in bearings and related services, many companies turn to SKF for new tools and solutions. The mounting of rolling bearings is no exception. With the explicit aim of developing a practical and accessible solution, Linus Waltherius, senior project manager at SKF Technology, set out to map the world of mounting issues. Quickly, a working hypothesis formed: what if you could get all the knowledge you need for successful mounting, in the palm of your hand?
This idea seemed to resonate with what people in the field were looking for. “When we asked our customers how we could use new technology to better support them when working with our bearings, their answers where very consistent: quicker access to product information and maintenance instructions,” Linus says.
Many interviews, workshops and tests later, the solution became SKF Bearing Assist – an easy to use mobile app that aims to ensure quick, correct and easy mounting through a step-by-step process through the whole mounting procedure.
The app provides a structured way of working. It’s easy to understand and use. I immediately provided my staff with mobile phones so they could start to document our maintenance work in the app. We also share it the with external fitters so they get guidance, which helps them complete their work with less support from us. And once they’re done we can go through a checklist in the app. So, I really enjoy this new way of working with the SKF Bearing Assist app.
Ove Jansson, Roll Shop Manager, Holmen Paper AB, Sweden
Every step of the way
The new digital tool is meant to support everyone who mounts a bearing. By entering the bearing designation or scanning the barcode on the packaging, the user can access product information and mounting instructions. Checking the bearing details to make sure the right bearing is selected before mounting is, as discussed above, crucial, and by searching for dimensions and bearings, users can select the appropriate bearing and also keep track of their most recent bearing exchanges.
The app also offers support around mounting preparations, including information about the right tools and equipment. In addition, there are check lists to make sure nothing is forgotten. “The new SKF Bearing Assist app not only lets you save time and effort when mounting bearings,” Linus explains, “it actually improves your mounting skills and methods.”
But it does more than that. Actually, the purpose of the app’s documentation features is to help establish efficient maintenance routines. For example, you can create a team and invite colleagues to exchange experience and knowledge. There’s also functionality for sharing mounting notes and photos within the team to hand over jobs without hustle. In short, SKF Bearing Assist covers everything from planning to completion and sharing, making sure the right information and instruction is always at hand for successful mounting.
A crucial insight driving the app development process was the industry’s increasingly harder struggle to recruit maintenance professionals. This meant a growing demand for effective digital tools supporting those lacking years of field experience. As Linus puts it, “We clearly needed to develop a tool that could turn new recruits into experts.”
Mounting is indeed a critical stage of a bearing’s lifecycle, affecting the productivity and reliability of industrial applications to an uncomfortably high degree. Now, as the solutions to many long-established mounting issues move into the digital domain, SKF Bearing Assist offers better and more accessible assistance for everyone – both veteran and rookie – who mounts or replaces an SKF bearing. “By providing more value and a better user experience to our customers, we’re aiming to strengthen our position as a leader in the bearing industry and being the preferred brand for the next generation of maintenance technicians,” Linus concludes.