Design
Kitchen footwork
New contracts
Audi AG SKF has signed contracts estimated at some 110 million euros with Audi for the delivery of components for a...
Getting big by going small
Having dominated the Indian compact car market for more than 20 years, Maruti Suzuki is today the country’s largest car...
Improved seals head unit for off-road vehicles
SKF’s new seals head unit is an integrated application for off-road vehicles such as enduro and cross motorcycles, snowmobiles and...
At the bottom of the sea
Magnetic bearings from the SKF subsidiary S2M have been selected to equip the compressors and high-speed motors of the Åsgard...
Flying without wings
The burgeoning market for advanced flight simulators is enabling a Swiss manufacturer to take off. In the small village of Pratteln outside...
Roller bearings for the High Roller
The American Bridge Company has contracted SKF to supply technological solutions for the Las Vegas High Roller, soon to be...
Hot applications run longer with graphite
Many bearings operate in very high temperature environments – but few lubricants can withstand the heat. SKF has developed bearing...
Weather or not
Sweden’s addition to the ranks of the world’s largest convertibles. The world's first retractable roof over a sports arena was built...
Homeward bound
Re-entry into the earth’s atmosphere is a dangerous phase of space flight. The European Space Agency’s IXV project is testing a...